Contact us

A new window will open A new window will open



Since refrigerators work continuously, it is important to reduce their power consumption. At the same time, the market demand for ample indoor space is driving the need for thinner heat insulators and smaller motors. Because refrigerators are used in homes, it is necessary to improve motor efficiency, even at low speeds, in order to reduce acoustic noise and vibration. An inverter controls a compressor. Various sensors and a microcontroller work in tandem to regulate indoor temperatures and humidity. The compressor driver consists of IGBTs or power MOSFETs (PWMOSFETs). Power factor correction (PFC) ICs or IGBTs are used in the power supply circuit to keep harmonics in the input current below the IEC limit.

Refrigerators Block Diagram

Click on the colored blocks to view recommended products.

Refrigerators Block Diagram

Communication Sensor System Control Motor Motor Heating Power Supply Power Management General-purpose
    TVS Diode for ESD Protection
  • WLAN
  • NFC


If you have any queries, click one of these links:

Technical queries
Queries about purchasing, sampling and IC reliability
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.