Contact us

A new window will open A new window will open

Toshiba Introduces Photorelays with up to 5A Drive Current for Replacing Mechanical Relays in Industrial applications

18th October 2016

New products deliver enhanced reliability and improved safety margins in compact DIP8 packages

Toshiba Electronics Europe has introduced three new compact, DIP8 package products to its line-up of photorelays that can replace mechanical relays in industrial applications. The new devices - which include an industry-leading[1] 5A large drive current  – will suit a variety of applications ranging from heating, ventilation and air conditioning (HVAC) systems to inverters, PLCs and automated test equipment (ATE).

Unlike mechanical relays, photorelays have no physical contacts that are subject to wear and deterioration. This contributes to greater reliability. Use of photorelays also helps support the development of smaller and thinner designs. A guaranteed pulsed ON-state current that is three times greater than that of the continuous ON-state current secures a margin for safety design.

Toshiba’s TLP3547 is a 60V product with an industry-leading [1] 5A (max.) large drive current. The TLP3548 is a 400V product with a 0.4A (max) drive current that offers high-speed switching of 1ms (max). The 600V TLP3549 is the industry’s first [2] photorelay to utilise a super-junction structure ‘DTMOS’ MOSFET and delivers a 0.6A (max) drive current.

All of the new photorelays have a minimum isolation voltage rating of 2500Vrms.

Notes:

[1] For photorelay products in DIP8 packages, as of July 19, 2016. Toshiba survey.

[2] For photorelay products, as of July 19, 2016. Toshiba survey.

TLP3547 More

TLP3548 More

TLP3549 More

News Links

      

  High Resolution Image (jpg)

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.