Contact us

A new window will open A new window will open

Toshiba Launches IoT Development Kit for Design of Bluetooth® Enabled Wearables

28th February 2017

Starter kit supports applications that need to process multiple sensor inputs

Toshiba Electronics Europe (TEE) has announced a comprehensive development kit that provides the hardware and software needed to create wearable devices that handle multiple sensor inputs. The EBTZ1041-SK-A1 'starter kit' supports the prototyping of highly integrated IoT wearable applications featuring the Toshiba TZ1000 ApP Lite™ family of IoT processors.

Toshiba's new kit incorporates the company’s TZ1041MBG 'sensor hub' application processor. This processor is based on a high-performance 32-bit ARM® Cortex®-M4F processor and acts as a hub to collect, process and store data from multiple sources. It then transfers the raw or processed data to external devices such as smartphones and tablets using an integrated Bluetooth® wireless communication function.

The EBTZ1041-SK-A1 evaluation board combines the TZ1041MBG processor with an Arduino UNO R3-compatible header that allows developers to connect to commercially available Arduino shields. In addition to the integrated Bluetooth®, a dedicated header to connect to Toshiba’s TC32306 single-chip RF transceiver further supports sub-GHz wireless communications. An on-board CMSIS-DAP debug interface is provided as standard. Alternative debuggers can be connected via the board’s 9-pin SWD connector.

Toshiba's TZ1041MBG allows peripheral devices and sensors - for example MEMS sensors such as atmospheric pressure sensors and moisture sensors – to be connected via various integrated USB, UART, SPI, I2C and 12-bit ADC interfaces. Other external sensors can be directly connected to the three input channels of the device’s integrated 24-bit high-resolution ΔΣADC - this allows for accurate measurement of biomedical signals including pulse rates and electrocardiograms. This accurate data is collected and processed by the high-performance ARM Cortex®--M4F with DSP instructions and a floating point processing unit. The processor also incorporates 288KB SRAM operating memory and 1MB NOR flash memory for storing program code and data. The integrated Bluetooth® LE controller and RF circuit - compliant with Bluetooth® Ver4.1 Low Energy standards - transfer raw and processed data to external equipment.

Other members of the Toshiba family are the TZ1011MBG, TZ1031MBG and TZ1021MBG. The first two also integrate accelerometer and gyroscope, the TZ1011 also contains a magnetometer sensors. The latter does not feature integrated sensors and BLE functionality.

As well as the starter kit hardware, wearables developers have access to Toshiba software algorithms for the TZ1000 series. These include Activity Monitoring, PPG (Photoplethysmography) Monitoring and ECG (electrocardiography) Monitoring.

Toshiba's EBTZ1041-SK-A1 'starter kit' is available immediately.

Further information is available at the following link: https://toshiba.semicon-storage.com/eu/product/assp/applite.html. This also provides access to the ApP Lite Developer Zone. Here developers can join Toshiba’s developers' web pages: register and get access to a wealth of development tools, BSP (Board Support Package), HcSDP (Health Care Software Development Platform), manuals, datasheets, reference designs and more.

Notes:

ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere. All rights reserved.

ApP Lite is a trademark of Toshiba Corporation.

The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc.

All other company names, product names, and service names may be trademarks of their respective companies

Contact Us More

The starter-kit supports easy and fast design in combination with our Developer Zone More

News Links

           

  High Resolution Image (jpg)

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.