Contact us

A new window will open A new window will open

Why does the LDO output voltage oscillate?

The LDO regulates its output voltage using negative feedback. The output voltage oscillates when the phase of the signal to detect changes in the output voltage (VOUT) lags by 180°, turning negative feedback into positive feedback. The LDO incorporates an error amplifier, a drive circuit for an output transistor, and the output transistor. The feedback loop has an inherent delay due to the capacitance and resistance of these circuits. If the loop has a gain, negative feedback turns into positive feedback when the phase delay due to this inherent delay reaches 180°, causing the difference between the output and reference voltages to be amplified.

For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.