Contact us

A new window will open A new window will open

What is the input-tolerant function?

The input-tolerant function blocks the current flowing from the CONTROL terminal to the input voltage (VIN) terminal when the CONTROL terminal voltage (VCT) is higher than the input voltage (VIN).

Input-tolerant function

Also see the following document and web page for a description of the input-tolerant function:
To perform a parametric search of load switch ICs with an output discharge function, click:
Other load switch ICs:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.