What is the value of the pull-down resistor connected to the active-High CONTROL terminal of load switch ICs?

Generally, load switch ICs incorporate a pull-down resistor between the CONTROL and GND terminals so that their internal circuitry remains stable in the event of the CONTROL terminal being open-circuited. Toshiba’s load switch ICs contain a MOSFET instead of a resistor as shown in Figure 1 in order to reduce control pull-down current (ICT). This MOSFET pulls down the CONTROL signal to GND with an almost constant current sink as shown in Figure 2.

Figure 1 Pull-down circuit between the CONTROL and GND terminals
Figure 1 Pull-down circuit between the CONTROL and GND terminals
Figure 2 Example of a CONTROL voltage vs. CONTROL current curve
Figure 2 Example of a CONTROL voltage vs. CONTROL current curve

Also see the following document and web page for a description of the CONTROL terminal:

Other load switch ICs:

A new window will open