Contact us

A new window will open A new window will open

Is a bypass capacitor required between the VCC and GND terminals?

For IC couplers with built-in amplifier circuit, internal oscillation may occur for such a reason as VCC voltage transient owing to load switching or power supply noise. In order to prevent it and realize normal operation, Toshiba recommends inserting a 0.1μF bypass capacitor with good high-frequency characteristics between VCC and GND and mounting it within 1cm of the pins. For some gate driver IC couplers, in order to control an impact attributable to a large fluctuation of the output current, Toshiba recommends mounting an about 1 μF bypass capacitor. For details, refer to individual data sheets.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.