How long does it take from when an input signal enters until the switch changes?

Turn-ON Time tON and Turn-OFF Time tOFF are defined and their information is provided. The switching time is greatly affected by the drive condition for IF at the input side, but it has a response rate in the range of 0.1–0.2ms to several ms.

A new window will open