How can I prevent the output voltage from overshooting following the application of the control voltage to an LDO?

To prevent the output voltage from overshooting, use an LDO with a soft-start or inrush current limiting function. The soft-start function raises the output voltage slowly after the control voltage is applied to an LDO.

To perform a parametric search of LDOs with a soft-start or inrush current limiting function, click:

For other LDO regulators, visit the main web page of LDO regulators at: