3글자 이상 입력하세요.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Select Product Categories
Select Application
Find everything you need for your next product design. Simply select an application and click through to the block diagram to discover our semiconductor solutions.
New Products / News
IoT (Internet of Things) is used to collect the data for optimizing various system control by monitoring all devices over the Internet. Since IoT sensors may be installed in locations where it is difficult to secure a commercial power supply, they must be operated by small battery so ultra-low power consumption while maintaining the sensor accuracy requires for the system. Toshiba offers a lineup of ultra-low-noise CMOS op-amps with low power operation, and power management ICs such as LDO regulators, which are ideal for these requirements. In addition, we have a lineup of MOSFET, SiC Schottky barrier diodes, and photocouplers that are used with the latest generation processes for AC-DC power supply. These products support the high performance of a variety of IoT sensor devices.