Contact us

Uma nova janela será aberta Uma nova janela será aberta

Air Conditioners

Air Conditioners

Air conditioners were the first major home appliance to use inverter control. Key semiconductor devices used for inverter control of a compressor motor include microcontrollers, insulated gate bipolar transistors (IGBTs) and photocouplers. Microcontrollers provide overall system control, pulse-width-modulation (PWM) generation and system protection functions. IGBTs and photocouplers reside in the inverter driver circuit and its interface, respectively. These days, more and more air conditioners feature a self-cleaning capability and a vector-controlled compressor motor for energy saving. Power factor correction (PFC) ICs or IGBTs are used in the power supply circuit to keep harmonics in the input current below the IEC limit.

Air Conditioners Block Diagram

Click on the colored blocks to view recommended products.

Air Conditioners Block Diagram

Communication Sensor Motor System Control System Control Interface Sensor Motor Solenoid Remote Controller Power Supply Power Management General-purpose
    TVS Diode for ESD Protection
  • WLAN

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.