Contact us

Uma nova janela será aberta Uma nova janela será aberta

Other power management

Overview

Of electronic devices, mobile devices such as smartphones and tablets are becoming more and more sophisticated. These devices require many types of power supplies tailored to each embedded function.
In response, Toshiba has continually released multiple-output power supply ICs. However, because of the rapid progress of mobile devices, even the latest multiple-output power supply ICs sometimes cannot meet customer requirements. In such cases, small LDO regulators and load switch ICs are used to provide individual voltages.
Nowadays, wearable devices and part of IoT devices are also battery-operated. This is spurring the demand for small LDO regulators and load switch ICs with low power consumption to improve battery life.

Block Diagram

file

Application

Application

Power management IC products

other02_en
other03_en

Documents

Application Note

Application Note
Name Outline Date of issue
Describes the key electrical characteristics of and evaluation boards for power multiplexers 9/2016
Describes the circuits, functions, electrical characteristics and usage considerations for load switch ICs 12/2012
Describes the circuits, functions, electrical characteristics and usage considerations for LDO regulators 12/2012

Catalog

Catalog
Name Outline Date of issue
Describes the lineups of Small Package(MOSFET/BJT/Diode/Linear IC/Logic/RF Device) 7/2019

Video


Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.