Contact us

Uma nova janela será aberta Uma nova janela será aberta

VR Head Mounted Display

VR Head Mounted Display

VR head mounted display(VR-HMD) is a device for immersive experience by using head mounted two displays of binocular disparity.
 

Toshiba offers the optimal portfolio of semiconductor devices for VR head mounted display applications, such as interface bridge of HDMI input or DP input, application processor for system control, LED driver for head tracking, wireless power charging, power solutions and circuit protection devices.

Block Diagram

(1) PC tethered VR-HMD/HDMI input

fig01_vr-hmd

LDO LDO Load Switch TVS TVS TVS TVS LED Driver Wireless Power Charger Serial Interface NAND Main Processor Interface Bridge

(2) PC tethered VR-HMD/DP input

fig02_vr-hmd

LDO LDO Load Switch TVS TVS TVS Bus Switch LED Driver Wireless Power Charger Serial Interface NAND Main Processor Interface Bridge

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.