Contact us

Uma nova janela será aberta Uma nova janela será aberta

Toshiba Memory Corporation Introduces World’s First* Enterprise-Class SSDs with 64-Layer 3D Flash Memory

Toshiba Memory Corporation (TMC) now sampling industry’s fastest4 SAS and enterprise NVMe TLC-based solid state drives

IRVINE, Calif. — August 7, 2017 — Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, today unveiled the development of two new flagship enterprise solid state drive (SSD) solutions, the TMC PM5 12Gbit/s SAS series and the CM5 NVM Express® (NVMe™)1 series. Development is expected to be completed in the fourth quarter. Both product lines are built with TMC’s latest 64 layer, 3-bit-per-cell enterprise-class TLC (triple-level cell) BiCS FLASH™2, making it possible for today’s demanding storage environments to expand the use of flash with cost-optimized 3D flash memory. With all-new, advanced features, the innovative CM5 and PM5 series raise the bar in performance capabilities and create new opportunities for businesses to leverage the power of flash storage.


Offering up to 30.72TB3 in a 2.5-inch form factor, the TMC PM5 series introduces a full range of endurance and capacity SAS SSDs enabling data centers to effectively address big data demands while streamlining storage deployments. With the industry’s first MultiLink SAS™4 architecture, the PM5 series is able to deliver the fastest performance the market5 has seen from a SAS-based SSD with up to 3,350 MB/s of sequential read and 2,720 MB/s of sequential write6 in MultiLink mode and up to 400,000 random read IOPS7 in narrow or MultiLink mode. The PM5 series’ 4-port MultiLink design is an additional technology to achieve high performance, close to PCI EXPRESS® (PCIe®)8 SSDs, enabling legacy infrastructures to increase productivity without having to be re-architected from the ground up. Furthermore, PM5 SSDs support multi-stream write technology, a feature that intelligently manages and groups data types to minimize write amplification and minimize garbage collection, translating into reduced latency, improved endurance, increased performance and Quality of Service (QoS).


As TMC’s next generation NVMe SSD, the dual-port PCIe Gen3 x4 CM5 is a full-featured enterprise SSD.  Like the PM5, it also supports multi-stream write technology. It is NVMe over Fabric-ready with scatter-gather list (SGL) and controller memory buffer (CMB) features. The CMB feature uses a part of DRAM on the SSD as host-system memory, reducing DRAM used load of host-side and it enables high speed as a system. Utilizing TMC’s BiCS FLASH 64-layer technology, the CM5 series has excellent performance with up to 800,000 random read and 240,000 random write IOPS for the 5 DWPD9 (drive writes per day) model and up to 220,000 random write IOPS for the 3 DWPD model, both with a maximum power draw of 18W. Additionally, the CM5 is being used as a platform to demonstrate and to enable the ecosystem around the Persistent Memory Region (PMR) capability. PMR enables customers to augment system memory with DRAM on the SSD without the use of expensive non-volatile DIMMs (NV-DIMMs). This feature makes it possible for a single SSD solution to provide both high performance storage and persistent memory to meet system performance requirements, while significantly reducing costs by moving metadata operations, such as logging, journaling and application staging to the SSD.


“We are proud to be first to market with new enterprise flash innovations to further broaden our enterprise SSD portfolio and re-writing the rules for enterprise SSDs using 3D TLC FLASH,” said Steve Fingerhut, senior vice president and general manager of Toshiba America Electronic Components, Inc. SSD business unit. “Toshiba’s customers demand more out of storage and Toshiba delivers enterprise solutions that fit application needs.”


“Broadcom and Toshiba have a long history of collaborating to maximize system performance and reliability for our server/storage OEMs and datacenter customers,” said Jas Tremblay, General Manager, Data Center Solutions Group at Broadcom. "Toshiba’s new PM5 SSD supporting MultiLink SAS enables system customers to experience the highest performance from the mature and reliable SAS ecosystem.”


PM5 12Gbit/s SAS SSDs will be available in capacities ranging from 400GB to 30.7TB with sanitize instant erase (SIE) and Trusted Computing Group (TCG). CM5 NVMe SSDs will offer capacities ranging from 800GB to 15.36TB with SIE and TCG. Both TLC-based product lines offer industry standard endurance ratings with 1, 3, and 5 DWPD options, and the PM5 has a 10 DWPD option available. 


The PM5 and CM5 series is sampling to select OEM customers and will be unveiled and demonstrated at the Flash Memory Summit in Santa Clara, CA, from August 8 to 10 in booth #407.  


For more information on Toshiba’s line of industry-leading SSDs, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html. To learn more about Toshiba’s storage solutions, follow @ToshibaStorage on Twitter.


*About Toshiba and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more. 


Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations that contribute to realization of a world where generations to come can live better lives.


To find out more about Toshiba, visit www.toshiba.co.jp/worldwide/about/index.html


*As of August, 2017, based on TMC survey

1NVM Express and the NVM Express logo are registered trademarks, and NVMe is a trademark of NVM Express, Inc.
2NAND/BiCS FLASH: Product density is identified based on the maximum density of memory chip(s) within the Product, not the amount of memory capacity available for data storage by the end user. Consumer-usable capacity will be less due to overhead data areas, formatting, bad blocks, and other constraints, and may also vary based on the host device and application.
3Definition of capacity: Toshiba Memory Corporation defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 230 bytes = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
4MultiLink SAS is a trademark of the SCSI Trade Association
5As of August 7, 2017, based on industry-published specifications, TMC survey
6Read and write speed may vary depending on the host device, read and write conditions, and file size.
7IOPS: Input Output Per Second (or the number of I/O operations per second)
8PCIe® and PCI EXPRESS® are registered trademarks of PCI-SIG
9DWPD: Drive Write Per Day. One full drive write per day means the drive can be written and re-written to full capacity once a day every day for five years, the stated product warranty period. Actual results may vary due to system configuration, usage and other factors

* All other company names, product names, and service names mentioned herein may be trademarks of their respective companies.


Information in this press release, including product, development completion time, pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.