Contact us

Uma nova janela será aberta Uma nova janela será aberta

Toshiba Announces 8TB High-Performance Internal Hard Drive

X300 Series HDDs offer high performance and reliability designed for professional systems, home media and gaming PCs.

IRVINE, Calif. — August 22, 2017 — Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, today announces the X300 3.5-inch1 internal hard drive in 8TB2 capacity. Compared to the P300 series with capacities up to 3TB, the X300 Series delivers extreme performance and robust capacity for creative and professional applications including graphic design, animation, photo and video editing, and PC gaming.

The new 8TB model features Toshiba’s cache technology, a self-contained cache algorithm with on-board buffer management, optimizes cache allocation during read/write to provide high-level performance in real time. The X300 Series is offered in 4TB, 5TB, 6TB and 8TB capacities, all with a higher 128MB cache than P300 series3, ensuring fast data access. Available in a 3.5-inch form factor, the X300 performs at 7200RPM and a SATA connection up to 6Gbit/s4. Compatible with most major brands of Serial ATA enabled desktop computers, the Toshiba X300 high-precision head positioning supported by advanced format technology (physical 4KB sector) and dual stage actuator technology delivers high storage density and capacity.

“Availability of the 8TB X300 Series is a testament to Toshiba’s commitment to growing the consumer HDD category and providing the tools needed to achieve varying professional workloads,” said Michael Cassidy, Vice President of Consumer HDDs at TAEC. “Toshiba offers a full internal HDD lineup that targets specific storage applications and grows with your gaming library and digital content.”

The new X300 will be available this month with a 2-year limited warranty5 at major retailers. For more information on Toshiba’s entire line of consumer storage solutions, visit: For more information on Toshiba’s full line of leading HDDs, please visit: To learn more about Toshiba’s storage solutions, follow @ToshibaUSA and @ToshibaStorage on Twitter.

*About Toshiba and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.  

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations that contribute to realization of a world where generations to come can live better lives.

To find out more about Toshiba, visit

1"2.5-inch" and "3.5-inch" mean the form factor of HDDs or SSDs. They do not indicate drive's physical size.
2Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240 bytes = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary..
3P300 series deliver 64 MB cache.
4Read and write speed may vary depending on the host device, read and write conditions, and file> 5Limited Warranty, full terms and conditions available at

Information in this press release, including product, development completion time, pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.