Contact us

Uma nova janela será aberta Uma nova janela será aberta

New ESD Bidirectional Protection Diode from Toshiba Designed for Mobile Devices

Housed in Ultra-Compact Package for Applications Requiring Small Footprint

IRVINE, Calif., September 14, 2017Toshiba America Electronic Components, Inc. (TAEC)* has introduced a new bidirectional electrostatic discharge (ESD) protection diode for semiconductor devices used in mobile device interfaces. The DF2B7ASL utilizes snapback characteristics, providing low dynamic resistance and superior protective performance to safeguard against static electricity and noise. Housed in an ultra-compact package (0.32x0.62mm), the DF2B7ASL is designed for applications with a small footprint, such as smart phones, tablets and notebook PCs.


Key Features

  • Protects devices with its high ESD performance. VESD=30kV at IEC61000-4-2 (Contact) and (Air)
  • Low dynamic resistance protects semiconductor devices from static electricity and noise (RDYN=0.2Ω (typ.))
  • Suitable for use with a 5V signal line (VRWM ≤ 5.5V)
  • Snapback characteristics realizing low clamping voltage protects semiconductor devices (VC = 11 V@IPP=4A (typ.))
  • Compact package is suitable for use in high density board layouts such as in mobile devices. SOD-962: 0.32×0.62mm size (Toshiba package name: SL2)


Main Specifications

Part
number

Absolute
maximum
ratings

Working
peak
reverse
voltage
max
(V)

Reverse
breakdown
voltage
(V)
@ IBR=1mA

Clamp
voltage
typ.
2
(V)
@ 1A

Dynamic
resistance
typ.
(Ω)
@ 8 to 16A

Total
capacitance
typ.
(pF)
@ 0V,
1MHz

Package

Remarks

Electrostatic
discharge
voltage
1
(kV)
@ 16A

DF2B7ASL3

±30

5.5

5.8 to 7.8

8

0.2

8.5

SOD-962
(SL2)

Bidirectional,
typical total
capacitance

DF2B7SL

±17

5.3

5.8 to 7.8

8

0.3

6

Pricing and Availability

The new ESD protection diodes are available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.


*About Toshiba and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more. 


Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations that contribute to realization of a world where generations to come can live better lives.


To find out more about Toshiba, visit www.toshiba.co.jp/worldwide/about/index.html


1IEC61000-4-2 (contact discharge)
2@TLP parameter: ZO=50Ω, tp=100ns, tr=300ps, averaging window t1=30ns to t2=60ns
3New product


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.