Contact us

Uma nova janela será aberta Uma nova janela será aberta

Toshiba Announces New 1TB Hard Disk Drive for Mobile Client Storage Applications

New MQ04 HDD Series model delivers 1TB capacity in a sleek, quieter design for portable PCs, game systems and other client storage applications

IRVINE, Calif. — SEPTEMBER 11, 2017 — Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, today announces its new MQ04 Series 1TB1 HDD, which is compatible with notebook PCs, game systems, all-in-one slim-line desktop systems, set-top box appliances, and other applications requiring high capacity and durability storage.


The MQ04 Series single-disk model delivers 1TB of data storage capacity in an ultra-compact 2.5-inch, 7mm height form factor. The drive’s 6 Gbit/s2 SATA interface and 5,400 rotational speed combined with a large 128MiB3 buffer and consistent seek performance, result in a 34 percent higher internal transfer rate performance when compared to the previous 1TB MQ01 Series models. The new model is also quieter and weighs less than prior generations. 


“Achieving 1TB per disk capacity is a big advancement in both value and performance, and without increasing weight in portable PCs,” said Scott Wright, Director of HDD Product Marketing at Toshiba America Electronic Components, Inc. “With a field-proven single disk 7mm design heritage, the new Toshiba MQ04 1TB model offers reliable performance and capacity at the leading edge of mobile client HDD technology and value.”  


Toshiba recently revealed that it was the fastest growing vendor in the HDD space for 20164 and the new MQ04 series 1TB model is another testament to Toshiba’s determination to meet customer demand with drives that offer variety, dependability, and efficiency for every need. General availability of the MQ04 1TB model shipment will start today. For more information on Toshiba’s line of industry-leading HDDs, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html. To learn more about Toshiba’s storage solutions follow @ToshibaStorage on Twitter.


About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more. 


Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations that contribute to realization of a world where generations to come can live better lives.


To find out more about Toshiba, visit www.toshiba.co.jp/worldwide/about/index.html


1Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240 bytes = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary
2Read and write speed may vary depending on the host device, read and write conditions, and file size.
3A kibibyte (KiB) means 210, or 1,024 bytes, a mebibyte (MiB) means 220, or 1,048,576 bytes, and a gibibyte (GiB) means 230, or 1,073,741,824 bytes.
4Worldwide 4Q16 HDD Shipment Results and Four-Quarter Forecast Update (Feb 2017 - Doc # US42306617)


Information in this press release, including product, development completion time, pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.