Contact us

Uma nova janela será aberta Uma nova janela será aberta

How does a boost converter work?

As the figure below shows, when the MOSFET is ON, current mainly flows through the coil and the MOSFET. Energy is accumulated in the coil during this time. The coil emits accumulated energy and suppresses changes of current. Current does not flow at the moment when the MOSFET turns OFF, but owing to the characteristic of this coil, current flows through a diode, and the capacitor is charged. Because of this phenomenon, output voltage exceeds input voltage.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.