Contact us

Uma nova janela será aberta Uma nova janela será aberta

Is there anything to keep in mind when using a sensorless DC motor?

Instead of detecting the rotor position using sensors (Hall elements or a Hall IC), a sensorless motor drive system monitors changes in the motor back-EMF voltage to predict the timing of current conduction. However, applications in which the motor RPM fluctuates considerably because of load variations make it difficult to predict this timing accurately, causing the motor to fall out of step. (The motor stops rotating.)
If the back-EMF voltage is insufficient, it is difficult to realize stable sensorless drive. When the back-EMF voltage is low at low RPM, motor operation tends to become unstable.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.