Contact us

Uma nova janela será aberta Uma nova janela será aberta

MOS devices are typically sensitive to electrostatic discharge (ESD). How should I protect MOSFETs against ESD?

Proper ESD protection is implemented in each device.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.