Contact us

Uma nova janela será aberta Uma nova janela será aberta

What causes motor failure and sine-wave distortion?

The motor may not work properly because of a noise on the Hall input. Add an RC filter to the Hall input for noise cancellation.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.