Contact us

Uma nova janela será aberta Uma nova janela será aberta

What are the applications of high-voltage IPDs?

High-voltage IPDs are designed to drive BLDC motors.

BLDC motors are used for a wide range of applications, including home appliances and industrial equipment, because BLDC motors provide high efficiency and long life.

The following figure shows major applications of high-voltage IPDs.

the applications of high-voltage IPDs

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.