Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is the bootstrap circuit in high-voltage IPDs?

A bootstrap circuit is used for the gate drive of the high-side (upper-leg) devices of a bridge circuit.

Generally, the gate of N-channel MOSFETs or IGBTs is driven at a voltage 10 to 15 V higher than the source voltage or emitter voltage. When a high-side N-channel device turns on, the source (or emitter) voltage becomes equal to that of the high-voltage power supply (VBB). Therefore, for the gate drive of the high-side device, a power supply with very high voltage, which is equal to the sum of VBB and the gate-source (gate-emitter) voltage, is required. The following shows a bootstrap circuit. When the low-side (lower-leg) device turns on, the bootstrap capacitor (C) stores charge, which is used to drive the gate of the high-side device.

Figure 1 Example of a bootstrap circuit

Figure 1 Example of a bootstrap circuit

Turning on the low-side device causes the bootstrap capacitor to be charged.

Turning on the low-side device causes the bootstrap capacitor to be charged.

The charge stored in the bootstrap capacitor is used to drive the high-side device.

The charge stored in the bootstrap capacitor is used to drive the high-side device.

Figure 2 Bootstrap operation

For High-voltage IPD’s bootstrap circuit, please refer to High voltage intelligent power device application note

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.