Contact us

Uma nova janela será aberta Uma nova janela será aberta

What type of Hall-effect devices is suitable for use with a high-voltage IPD?

To use our high-voltage IPD for square-wave drive (TPD415x series), select indium antimonide (InSb) Hall-effect devices with high output voltage.

Set the peak output voltage of Hall-effect devices above 300 mV.

The circuit, operation and usage of the high-voltage IPD are also described in "High voltage intelligent power device application note“. Please also refer to this document.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.