Contact us

Uma nova janela será aberta Uma nova janela será aberta

How can I calculate current and power consumption?

Broadly speaking, the power consumption of an LED driver consists of two factors: the power consumed due to the IC bias current and the power consumed due to current flowing through the output section. Both these factors are affected by the drive voltage and the duty cycle. For details of how to calculate the power consumption of an LED driver, see the appropriate datasheet or contact us.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.