Contact us

Uma nova janela será aberta Uma nova janela será aberta

You have announced that the TB62705CFG and TB62725BFG 8-channel LED drivers will be discontinued. Do you have any replacements for these devices?

The TB62777FG is recommended as a replacement for these LED drivers.
It should be noted, however, that they differ in the output drive current range. For details, see the datasheet or contact us.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.