Contact us

Uma nova janela será aberta Uma nova janela será aberta

How can a low-noise power supply be created using an LDO regulator?

If input voltage (VIN) has noise such as ripples, it is advisable to select an LDO regulator with a high ripple rejection ratio (R.R.).

R.R. is a figure of merit that represents the capability of an LDO regulator to filter out the ripples superimposed on VIN from the output.

Use R.R. as a guide when using an LDO regulator in analog and other highly noise-sensitive circuits. In cases where an LDO regulator is preceded by a DC-DC converter, an LDO regulator with a higher R.R. is more suitable for CMOS sensor and other high-precision analog circuits because a high-R.R. LDO regulator provides an excellent noise suppression capability. The ripple rejection ratio is calculated as follows:

Ripple rejection ratio

R.R. varies with ripple frequency. R.R. decreases as ripple frequency increases.

The R.R. curve shown in Figure 2 indicates that 200-Hz ripples can be suppressed to roughly 1/30000th whereas 100,000-Hz ripples can be suppressed to only roughly 1/800th.

The ripple rejection ratio is also called the power supply rejection ratio (PSRR) or the supply voltage rejection ratio (SVRR).

Figure 1 Ripple rejection
Figure 1 Ripple rejection

Figure 2 Ripple rejection ratio (R.R.) vs. frequency
Figure 2 Ripple rejection ratio (R.R.) vs. frequency

For LDO’s ripple rejection ratio, please refer to
To perform a parametric search of LDO regulators with a high ripple rejection ratio, click:
For LDO regulators with a high ripple rejection ratio, click:
For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.