Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is the resistance of the pulldown resistor connected to the CONTROL pin of the LDO regulator?

Generally, LDO regulators have a pulldown resistor between the CONTROL and GND pins so that their internal circuitry remains stable in the event of the CONTROL pin being open-circuited.

However, our LDO regulators have a MOSFET instead of a resistor as shown in Figure 1 in order to reduce control pulldown current (ICT). This MOSFET pulls down the CONTROL pin to GND with an almost constant current sink.

Figure 1 Pulldown circuit between the CONTROL and GND pins
Figure 1 Pulldown circuit between the CONTROL and GND pins

Figure 2 CONTROL pin voltage vs. CONTROL pin current
Figure 2 CONTROL pin voltage vs. CONTROL pin current

For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.