Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is the thermal shutdown (TSD) that is available with LDO regulators?

The thermal shutdown (TSD) function monitors the chip temperature of an LDO regulator and turns off its output to prevent chip degradation or destruction in the event of an excessive rise in chip temperature caused by a shorted load, an output-to-GND short-circuit, a rise in the ambient temperature, or self-heating.

When TSD is tripped, the output turns off, causing chip temperature to decrease. TSD has a hysteresis. The output automatically recovers normal operation when the chip temperature drops to the TSD recovery temperature.

Figure 1 Example of thermal shutdown characteristics of an LDO regulator
Figure 1 Example of thermal shutdown characteristics of an LDO regulator

To perform a parametric search of LDO regulators with a thermal shutdown function, click:
For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.