Contact us

Uma nova janela será aberta Uma nova janela será aberta

What voltage is required at the CONTROL terminal to enable an LDO?

To enable an LDO, apply a voltage in the range specified as “Control voltage (ON)” (VCT(ON)) to the CONTROL terminal. Ensure that the input voltage (VIN) is equal to or higher than the CONTROL terminal voltage (VCT).

CONTROL terminal voltage

For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.