Contact us

Uma nova janela será aberta Uma nova janela será aberta

Why is the output of an LDO disabled when its input voltage decreases?

One of the possible causes of this is the tripping of undervoltage lockout (UVLO*). When the input voltage of an LDO drops to the predefined threshold, UVLO disables the LDO to prevent false operation. The LDO is re-enabled when the input voltage rises above the recovery threshold. ULVO has a hysteresis.

* UVLO: Under Voltage Lock Out

Figure 1 Operation of undervoltage lockout (UVLO)
Figure 1 Operation of undervoltage lockout (UVLO)

For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.