Contact us

Uma nova janela será aberta Uma nova janela será aberta

Large inrush current flows when an LDO is enabled. What can I do to prevent this?

To reduce inrush current, use an LDO with a soft-start or inrush current limiting function. The soft-start function raises the output voltage slowly and limits inrush current after the control voltage is applied to an LDO.

To perform a parametric search of LDOs with a soft-start or inrush current limiting function, click:
For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.