Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is the purpose of the capacitor connected to one of the external resistors for an adjustable-output LDO?

The output voltage of an adjustable-output LDO is programmable via two resistors. The capacitor connected to the upper resistor (R1) is called a feedback capacitor (CFB). It is added to prevent oscillation, improve load transient response, and increase the ripple rejection ratio (R.R.) (also known as the power supply rejection ratio or PSRR for short). CFB and R1 introduce a zero and thus provide lead phase compensation, increasing an oscillation margin and improving load transient response.

feedback capacitor

To view the lineup of adjustable-output LDOs to which a feedback capacitor (CFB) can be connected, click:
For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.