Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is active clamping available with low-voltage IPDs?

When a low-side switch drives an inductive load, a high voltage is applied to the output terminal because of the back-EMF energy induced when the switch turns off. This back-EMF energy might degrade or damage the IPD.

Active clamping is a protective function to absorb the back-EMF energy incurred by the turn-off of the low-side switch. Active clamping also eliminates the need for freewheeling diodes (FWDs) that return back-EMF energy to a power supply.

Configuration of an  active clamping circuit

Figure 1 Configuration of an active clamping circuit

Operation of active clamping

Circuit

Active clamping period

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.