Contact us

Uma nova janela será aberta Uma nova janela será aberta

Is it OK to connect capacitors to the output lines?

There is a limitation to the maximum capacitance values at the output lines, which varies with conditions and differs from device to device. Contact us and allow for design margins.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.