Contact us

Uma nova janela será aberta Uma nova janela será aberta

Is it OK to make deliberate use of the equivalent diode structure between the drain (D) and the source (S)?

Typically, the DMOS output section has an equivalent parasitic diode structure. Read the handling precautions.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.