Contact us

Uma nova janela será aberta Uma nova janela será aberta

Are there any reasons why forward transfer admittance, |Yfs|, is not specified in datasheets?

Also called transconductance (gm), |Yfs| is the ratio of the drain current variation at the output to the gate voltage variation at the input and is defined as |Yfs| = ∆ID / ∆VGS. Therefore, |Yfs| can be read from the ID-VGS curve or the VGS-based ID-VDS curve shown in datasheets.
You should read a |Yfs| value under actual usage conditions from these performance curves rather than using a |Yfs| value under the predefined conditions for the Electrical Characteristics table. That is why |Yfs| is not specified in datasheets.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.