Contact us

Uma nova janela será aberta Uma nova janela será aberta

Is the MOSFET drive current necessary?

For bipolar transistors, a large base current is required to maintain low on-voltage. However, since the MOSFET is a voltage control element, it can drive with small power sufficient to charge the gate. But because the input capacitance (Ciss) of the power MOSFET is rather large for high-speed switching, it is necessary to quickly charge the input capacitance with a low-impedance drive circuit.

For an indication of the gate current required for charging, it is possible to calculate the drive current simply by using the Qg characteristic prescribed on the data sheet. The required switching time is “t (desired)” (for example ton or toff), which becomes the following expression.
Ig=Qg/t(desired)

Electrical Characteristics: Power MOSFET Application Notes (PDF:1,092KB)
https://toshiba.semicon-storage.com/info/docget.jsp?did=13415

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.