Contact us

Uma nova janela será aberta Uma nova janela será aberta

Is the on-state resistance of a MOSFET dependent on temperature?

The MOSFET has a positive temperature coefficient. Since values of coefficients depend on the drain-source breakdown voltages and the process, it is necessary to confirm with the data sheet etc. When performing thermal design / circuit design, please consider this temperature fluctuation.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.