Contact us

Uma nova janela será aberta Uma nova janela será aberta

MOS is sensitive to static electricity. How do you protect MOSFETs from static electricity?

If static electricity is applied to the gate when mounting the board, the gate oxide layer may be destroyed. Therefore, some products include a diode for protection against static electricity between the gate G and source S of the MOSFET.
Please check the datasheet.

Also, when measuring or mounting, etc., please handle ESD by using a wristband etc.
Zener diode for electrostatic protection

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.