Contact us

Uma nova janela será aberta Uma nova janela será aberta

How to calculate the avalanche energy.

Figure 1 shows the avalanche measurement circuit and Figure 2 shows the avalanche voltage and current waveforms.
Avalanche energy EAS is calculated by using following formula.

アバランシェ測定回路
          1                   BVDSS
EAS= ー LIAS2  ―――――――
          2                BVDSS -VDD
EAS : Avalanche energy
IAS : Avalanche current
BVDSS : Drain-source avalanche voltage
VDD : Supply voltage
アバランシェ波形


Avalanche ruggedness is the allowable energy in a single pulse.

For MOSFET’s avalanche, please refer to “Maximum Ratings: Power MOSFET Application Notes

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.