Contact us

Uma nova janela será aberta Uma nova janela será aberta

What are the capacitance characteristics of MOSFET.

Ciss, Crss and Coss are all important factors that influence switching characteristic of MOSFET.

  • Ciss: input capacitance (Ciss=Cgd+Cgs)
    ⇒Sum of gate-drain and gate-source capacitance. It influences delay time. The greater Ciss, the longer the delay time.
  • Crss: Reverse transfer capacitance (Crss=Cgd)
    ⇒Gate-drain capacitance. The greater Crss, the worse the drain current rising characteristics, which is disadvantageous for MOSFETs’ loss. Low capacitance is needed for high-speed driving.
  • Coss: Output capacitance (Coss=Cgd+Cds)
    ⇒Sum of gate-drain and drain-source capacitance. It influences turn-off characteristic and loss with light load. The greater Coss, the lower the turn-off dv/dt, which is advantageous for noise. But loss with light load increases.
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.