Contact us

Uma nova janela será aberta Uma nova janela será aberta

What does the dv/dt of the MOSFET mean?

The dv/dt of the MOSFET is the changing rate of the drain-source voltage during the switching transient.

If dv/dt is too large, ringing may occur, possibly leading to MOSFET damage.

Therefore, dv/dt ruggedness values are specified for some MOSFETs.


For MOSFET’s ringing, please refer to “Parasitic Oscillation and Ringing of Power MOSFETs:Power MOSFET Application Notes.”

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.