Contact us

Uma nova janela será aberta Uma nova janela será aberta

Can bias resistor built-in transistors (BRTs) be used for general amplification purposes?

Because BRTs are designed for a digital operation, they are not suitable for a linear (analog) operation. You might be able to use those BRTs that have only a bias resistor, R1, for amplification, but a board design should be fully verified empirically.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.