Contact us

Uma nova janela será aberta Uma nova janela será aberta

Is the specified power dissipation the sum of the transistor and the bias resistors?

Yes, the specified power dissipation is the sum of the power dissipation of both a transistor and the bias resistors.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.