Contact us

Uma nova janela será aberta Uma nova janela será aberta

Example of measurement of the key bipolar transistor characteristics

Example of IC-VCE measurement

The IC-VCE test requires pulse measurement.

Example of DC current gain (hFE) measurement

The hFE test requires pulse measurement.

Example of measurement of collector-emitter saturation voltage, VCE(sat)

The VCE(sat) test requires pulse measurement.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.