Contact us

Uma nova janela será aberta Uma nova janela será aberta

Transient thermal resistance vs. safe operating area

Thermal resistance is calculated as a rate of change of temperature caused by a single pulse with respect to power dissipation. Transient thermal response is a response of a device to a single pulse expressed in terms of the pulse duration.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.