Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is the function of BJTs?

They change small signals to large signals. This is called amplification. The ratio of collector current IC and base current IB (IC/IB) is called DC current gain, denoted as hFE.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.