Contact us

Uma nova janela será aberta Uma nova janela será aberta

What kinds of bipolar transistors (BJTs) exist?

There are two types of bipolar transistors:  NPN type and PNP type. The NPN-type lineup ranges from high- to low-voltage products, and the PNP-type lineup includes products under 400 V. (Products under 200 V are widely available.)

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.