Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is an IGBT?

IGBT stands for insulated-gate bipolar transistor. It is a bipolar transistor with an insulated gate terminal. The IGBT combines, in a single device, a control input with a MOS structure and a bipolar power transistor that acts as an output switch. IGBTs are suitable for high-voltage, high-current applications. They are designed to drive high-power applications with a low-power input.
Thus, typical applications of IGBTs include induction cooktops.

Example of an N-Channel IGBT

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.